WebClient login screen has the TAC webClient background, but no login fields

Issue

WebClient login screen has the TAC webClient background, but no login fields

Product Line

Andover Continuum

Environment

webClient

Cause

This typically happens when webclient has been installed prior to IIS, so .Net framework does not get registered with IIS.

Resolution

 The resolution is to run the regiis.exe command as follows:

For Windows 2000 Professional it is:
"c:\WinNT\Microsoft.NET\Framework\v1.1.4322\aspnet_regiis.exe -i"
"c:\WinNT\Microsoft.NET\Framework\v2.0.50727\aspnet_regiis.exe -i"

For Windows XP Professional, Windows Server 2003 it is:
"c:\windows\Microsoft.NET\Framework\v1.1.4322\aspnet_regiis.exe -i"
"c:\Windows\Microsoft.NET\Framework\v2.0.50727\aspnet_regiis.exe -i"

Once this command is run the normal login prompt will be presented.