Issue
USB Prox enrollment reader for I/NET Seven
Environment
I/NET Seven
Cause
I/NET supports the use on an Enrollment reader via the Hosts PC Serial port, most PC's no longer have serial ports. One solution is to use a USB supported reader which can be sourced by the supplier listed in the resolution
Resolution
The USB enrollment reader is made by RF Ideas. It is very easy to program for use in the I/NET Seven System. After you program certain steps it becomes a "Plug and Play" device at the job site. To set up this USB reader please consult this whitepaper.