Issue
"Field Unit Not Configured" when commissioning controller or network under a Xenta Server
Environment
- Xenta Server
- Xenta 511, 527, 701, 711, 721, 731, 913
Cause
The LonWorks Network object is not recognized correctly by the Xenta Server.
Resolution
- Create a new device "Communication Port - Echelon - LTA".
- Drag the "LonWorks Network" object on to the LTA port.
- Then drag the "LonWorks Network" object back on to the Xenta Server object.