Issue
In Niagara R2, device objects are not updating. Bundles were used to speed the linking to graphics.
Environment
Niagara R2
Cause
The device objects are in bundles.
Resolution
Only native Niagara objects should be placed in bundles. This includes the Niagara AO, BO, AI, BI, and logic (if desired). Due to the nature of bundles they execute at their own rate. This interferes with the normal execution of BACnet, LON, GCM, ASD, DMS, MS and other hardware objects.
For additional information on the use of bundles refer to The Standard Reference Manual pages 7-14 through 7-21 and pages 5-1 through 5-6 of the Web Solutions Guide.