Adding a BCX1-CR-32-INF controller into Cyberstation and the drop down list does not show this as an option

Issue

Adding a BCX1-CR-32-INF controller into Cyberstation and the drop down list does not show this as an option

Product Line

Andover Continuum

Environment

  • BCX1-CR-32-INF
  • CyberStation

Cause

In CyberStation when adding a controller to the system the drop down list will only show Model numbers and will not show the part number.

Resolution

See below for examples:

  • BCX1 Router Only Model Number = 4000
  • BCX1 Bacnet Version Model Number = 4040
  • BCX1 Onsite Version Model Number = 4020
  • BCX1 Infinet Version Model Number = 9640 
  • 8Meg Netcontroller Model Number = 9900
  • 4Meg Netcontroller Model Number = 9940
  • 2nd Gen Netcontroller Model Number = 9680
  • ACX2 (8 Door) Model Number = 5740
  • ACX2 (4 Door) Model Number = 5720