Issue
Does Windows XP Service Pack 3 (SP3) cause a problem with SIGNAL XP?
Environment
- SIGNAL XP computer
- Service Pack 3
- Service Pack 2
Cause
Any known issues with the SP3 helps if updating is necessary.
Resolution
The impact of SP3 on SIGNAL XP is not known. SIGNAL XP has been field-tested with Windows XP Service Pack 2 and the only issue identified was recognition of the Security Plug (see TA06-03). No other anomalies have been observed. There are no plans to validate SIGNAL XP with this new service pack. It is recommended that all SIGNAL XP computers maintain Windows XP at service pack 2.