Issue
Trend Log pages, Time Object pages, Alarm pages and Value pages in a TAC Xenta 721 project.
Product Line
TAC Vista
Environment
TAC Xenta 721
Cause
XBuilder allows for the creation of some additional objects in a Xenta 721 project for use with the OP7, not to be visible in a web browser or Vista Workstation.
Resolution
In the XBuilder 5.1.0 you can add Trend Log pages, Time Object pages, Alarm pages and Value pages in a TAC Xenta 721 project. These pages are only for use in the OP7. Unfortunately, they are visible in the TAC Vista database and the pages do not work in Vista. If you use IE to browse the Xenta 721, you can not see the pages. These pages should not be visible in TAC Vista. This was reported as a bug and will be corrected in later versions.