Xenta 700 Menta viewer in Internet Explorer displays some blocks at half-size

Issue

 

Xenta 700 Menta viewer in Internet Explorer displays some blocks at half-size

Product Line

TAC Vista

Environment

  • Xenta Server
  • Xenta 701, 711, 721, 731
  • Menta
  • Internet Explorer

Cause

Illegal characters in the description field of the point has caused problems with the web interface live Menta viewer.

Resolution

Verify that there are no strange characters in the description field of the point. In the most recent case, the = sign caused the block to shrink.