Issue
SNVT_press_p will not display correctly in Imperial units on a TGML graphic on a Xenta Server
Product Line
TAC Vista
Environment
- Xenta Servers
- Xenta 511, 527, 711, 731
Cause
There is a bug with the TGML graphic editor that causes a SNVT_press_p to only display in the SI units of pascals.
Resolution
Until this issue is corrected you can manually convert the value on the graphic page using a JavaScript.
This Pascal to H2O Snippet can be used to modify a numeric or text presentation object.