Issue
What PDAs (Personal Digital Assistants) are available for use with Sigma?
Environment
Sigma
WINCE
PDA
Cause
Supported PDA devices
Resolution
Version 4.01 WinCE (Build 3.36.24) software supported Dell Axim X51, X5, X3 PDAs which are now obsolete.
The software was expected to work on other compatible PDAs providing they were running Windows Pocket PC 2002/3 or Windows Mobile Version 5.
Version 4.04 WinCE software supports the following... Dell™ Axim™ X51 with Windows Mobile 5.0 iPAQ hx2490b with Windows Mobile 5.0 iPAQ 114 and the iPAQ 214 with Windows Mobile 6 Advantech TPC-30T panel mounting device with Windows CE 5.0.