Issue
Is Sigma IC-Gen DDE release 3.10 compatible with Sigma 4.04?
Environment
- Sigma IC-Gen DDE release 3.10
- Sigma 4.04
Cause
The release note for IC-Gen V3.10 states:
"This product has now been rebranded to reflect TAC ownership and reissued as release 3.17 (Build 3.34.14). All functionality is the same and this release note is applicable to both Invensys and TAC versions"
Resolution
Version V3.10 is in fact V3.17 and is compatible.