Issue
When interfacing Veris pressure transmitters (PXP-xx-02S-T1) with a 0 to 5 vdc output signal to a universal input of a MNL controller instead of seeing 0 vdc with 0 pressure the UI is seeing .5 vdc.
Environment
- Veris pressure transmitters (PXP-xx-02S-T1)
- MNL Controller
Cause
This is a compatibility issue with the Veris transmitters.
Resolution
Veris Technical Support suggests putting a 2.2k ohm resister across the OUT and COM of the transmitter. This has been confirmed to resolve the issue by field personnel.