Issue
A Niagara R2 Enterprise Server with a large number of alarms and archived data is no longer needed. How can all this data be removed quickly?
Environment
Niagara R2 Enterprise Server
Cause
Delete unused alarms and archived data on Enterprise Server station.
Resolution
This data is stored in the "app" folder on the Enterprise Server station. Using Windows Explorer go to Niagara > r2.301.522 > stations > "Station name". Rename or delete the "app" folder and restart the Enterprise Server. When Niagara discovers there is no "app" folder it will create a new, empty one.