The MN300 with an Slink sensor supported setpoint adjustments of 0.1 unit resolution. MN350, MN450, MN550 and MN650 with firmware version 2 and 3 only allowed 1.0 unit resolution.

Issue

The MN300 with an Slink sensor supported setpoint adjustments of 0.1 unit resolution.
MN350, MN450, MN550 and MN650 with firmware version 2 and 3 only allowed 1.0 unit resolution.
 

Product Line

Satchwell MicroNet

Environment

  • MN350
  • MN450
  • MN550
  • MN650

Cause

0.1 unit resolution is not supported on MN350, MN450, MN550 and MN650 with firmware version 2 and 3.

Resolution

MicroNet 50 controller Firmware version 5 released August 2008, when used with an updated Slink2.FCG file for VisiSat 2.1 Build 148 now supports 0.1 unit resolution changes.

The Slink2.FCG file is available for download from Exchange on line.

Additional information can be found in TPA-LOND-08-0014.00

Updated January 2014.
The MicroNet 50 series range MN350,450,550,650 LCD and Touchscreen have been withdrawn from sale.
Currently no direct replacement is offered.
The IAC 420, 600 and Touchscreen are not effected and remain available.