Can a graphical indicator be placed on a Niagara G3 graphic to indicate when a point is overridden, analog or binary?

Issue

Can a graphical indicator be placed on a Niagara G3 graphic to indicate when a point is overridden, analog or binary?

Product Line

TAC I/A Series

Environment

Niagara G3

Cause

By default, the StatusEffect setting is turned off (None). Change StatusEffect to Color to enable the graphical indicator.

Resolution

In the properties of the BoundLabel, set the StatusEffect attribute to Color (default is None). This will cause the object to turn purple (the default color) when it is overridden.