Issue
What is the Analog to Digital Output resolution of the MNL controllers?
Environment
MNL Controllers
Cause
Analog/Digital conversion resolution
Resolution
The MNL controllers (with the exception of the MNL-800) have a 10-bit equivalent UI resolution and an 8-bit output resolution.
The MNL-800 has a 12-bit equivalent UI resolution and an 8 bit output resolution.