Issue
Can the MNB controllers be powered by DC voltage?
Environment
- MNB controllers
- DC voltage input
Cause
Using DC voltage is not recommended or supported.
Resolution
The MNB controllers are not specified for DC operation and all agency approvals were submitted using a power source of 24 VAC 50/60 Hz.