Issue
How can a DMS-35, DMS-350A or DMS-3500 be connected to a Niagara R2 UNC-520 RS-232 port?
Environment
- Niagara R2 UNC-520
- DMS-35
- DMS-350A
- DMS-3500
Cause
To use a DMS with Niagara R2, connect using a pre-built adapters and silver satin cables.
Resolution
Pre-built adapters and silver satin cables for this type of connection are available for order.
The RJ-45 to DB-9 adaptor (UNCC-405) will interface to the DMS-350A and DMS-3500 panels.
The RJ-45 to DB-25 adaptor (UNCC-430) will interface to the DMS-35 panel.
A series of pre-terminated silver satin cables are available in three standard lengths:
- CBL-RJ45-4 Silver satin patch cable, 4 feet in length
- CBL-RJ45-10 Silver satin patch cable, 10 feet in length
- CBL-RJ45-25 Silver satin patch cable, 25 feet in length