Issue
Filter an alarm listview by EventNotification
Environment
Alarm Listview
Cause
The way to do this is to create a listview of class AlarmEvents and put the columns you want displayed on the columns tab.
Resolution
- To set up the filtering go to the Qualifiers Tab and under the database section select the checkbox "Advanced Database Qualifier".
-
In the qualifier box you will need to type in the statement below
EventNotificationClassID is like (put full path and name of the EventNotification here) id
- You need to manually type the above in the qualifier box because if you use the wizard the attribute is not listed correctly.