Templates cannot be changed for personnel because the option is grayed out in the Personnel Manager

Issue

Templates cannot be changed for personnel because the option is grayed out in the Personnel Manager

Product Line

Andover Continuum

Environment

Personnel Manager

Cause

This is an issue that was fixed in 1.82 and above.

Resolution

There are a couple of work arounds for this issue:

  1. Go into each template and select the Attribute data source tab
  2. Go to RefTemplate and change it from InheritFromTemplate to CopyFromTemplate
  3. Go back to the personnel and the ability to switch to other templates works


The other option is to switch the Personnel Manager to False in the Cyberstation preferences to use the Personnel Editor.
This is not an issue in 1.82 and above.