Issue
Tried to add a holiday event to a Niagara R2 calendar and received the error:
"Cannot add entry" /tridium/props/error.properties#error.E_CALENDAR_FULL
Environment
Niagara R2
Cause
There is a 50-event limit hard coded into the R2 schedule object.
Resolution
One solution is to use multiple Calendar objects.