Issue
Using the %D and %N on the FeedBack tab of an AlarmEnrollment and it is not filling in the Name or Description of a point.
Product Line
Andover Continuum
Environment
- Continuum Cyberstation
- Alarm View
Cause
Enhanced Alarm Logging has not been enabled.
Resolution
Make sure that you have selected Enhanced Alarm Logging on the Database Initialization screen. This is a requirement to use %D and %N in AlarmEnrollments.