Issue
Can the Network 8000 Microflo or CVV-80000 series controller be integrated using the Niagara R2 GCM driver?
Environment
- Niagara R2
- Network 8000
- CVV-80000
Cause
Information on integrating Network 8000 Microflo or CVV-80000 series using GCM driver
Resolution
Yes. Architecturally, it connects to the GCS bus of a GCM-84000 controller. The GCM database will contain VVBOX blocks which interact with the Microflo controllers. The VVBOX block can be read from and written to using GcmGeneric objects in a UNC station.