What's the latest version available in Pocket I/A? What make/model of handheld device was used in testing?

Issue

What's the latest version available in Pocket I/A? What make/model of handheld device was used in testing?

Product Line

TAC I/A Series

Environment

Pocket I/A

Cause

Would like to confirm the device is running the latest version of Pocket I/A.

Resolution

Pocket I/A Version 4.1 (Release B) is an update to previous versions of Pocket I/A to support the Microsoft Windows Mobile 5.0 Operating System used with newer handhelds.

The features and applications in previous versions of Pocket I/A will continue to operate in Pocket I/A Version 4.1 (Release B).

This version was tested using an HP IPAQ HX 2490B with MSMobile 5.0 operating system. Pocket I/A 4.1 can be downloaded from The Exchange Download Center.