Issue
What BACnet Command priority does a Cyberstation program use in changing value of BACnet points?
Environment
Cyberstation
Cause
Change the value of BACnet points
Resolution
When you use the WriteProperty() function, you must use the BACnet path of the object for WriteProperty() function.
- If the priority# is given in the WriteProperty() function, it sets the value of the point with the given priority#.
- If the priority# is not given in the WriteProperty() function, it sets the value with priority#16 by default.
When you don't use WriteProperty() function.
- If you use BACnet path ( Ex; BACnetDevices\BCXName\MyNum = 12.340), it sets the value with the priority# that is defined in the attribute of BACnet Command Priority for Cyberstation Programs in the BACnet Preferences.
- If you use Infinity path ( Ex; MyNetworkName\BCXName\MyNum = 12.340), it sets the value with priority# 10 by default.