Issue
Editing any time schedule weekly charts in Vista Webstation 4.5 results in the schedule being ON ALL DAY regardless of what changes were specified in the editor.
Environment
TAC Vista Webstation 4.5
Cause
Webstation is configured to use the wrong ASP.NET version.
Resolution
- Open IIS Manager
- Open the properties window of the Webstation application by right clicking on it.
- On the ASP.NET tab change the version to 1.1.4322 and click OK.
-
Stop the website and restart it in IIS Manager and the problem will now be fixed.