Will VisiSat work with Windows Vista?

Issue

Will VisiSat work with Windows Vista?

Product Line

Satchwell MicroNet

Environment

  • VisiSat
  • Windows Vista

Cause

Compatibility with Microsoft OS

Resolution

VisiSat Version 2.1 build 148 service pack 1 can either be used on a computer running Windows XP Pro with Visio 2003 or it can be used on a computer running Windows Vista with Visio 2007.

As detailed in the VisiSat 2.1 Configuration Tool Datasheet, available via Exchange OnLine, where you will also find the Installation/User's guide and the VisiSat Engineering Guides.

VisiSat Version 2.1 Build 148 service pack 1 is available for download via Exchange OnLine.
Note: File size = 41.5 Mb.