Issue
The MNB-1000 mounting base, manufactured before January 2009, does it comply with the UL 864 standard?
Environment
- MNB-BASE-1000
- UL 864
Cause
Information on MNB-1000 compliant with the UL 864 standard.
Resolution
The MNB-BASE-1000 has electronics on it that cannot be used for smoke control if it has a manufactured date prior to receiving UL 864 certification (January 2009).