When the remote I/O modules (MNB-1000-15) are powered for the first time, the status LED stays blinking red.

Issue

When the remote I/O modules (MNB-1000-15) are powered for the first time, the status LED stays blinking red.

Product Line

TAC I/A Series

Environment

MNB-1000-15

Cause

This is normal operation.

Resolution

  1. When the associated MNB-1000 receives a database configured with remote I/O modules, it will initiate communication to the remote I/O modules.
  2. If it is successful, then the status LED with turn green.