Issue
With InVue Developer, adding dates to a NETWORK 8000 Holiday Schedule OCX, the year displays as "20" instead of "09" (for 2009) or "10" (for 2010).
Environment
- Windows NT
- Windows 2000
- InVue Developer
- NETWORK 8000 Holiday Schedule OCX
Cause
By default, Windows NT and Windows 2000 display the short date as "M/d/yyyy"
Resolution
- Go to Windows Control Panel > Regional Options > Date tab
- Change the Short date format to "MM/dd/yy"
- Click OK.