Issue
When using Workplace Tech 5.x, after clicking on a help button assigned to various objects, the following pop-up message appears: “Cannot find the WPTech5.hlp file. Do you want to try to find this file yourself?”
Environment
WorkPlace Tech 5.x
Cause
The file in question was removed, but not all shortcuts were updated to point to the new document.
Resolution
The link should have pointed to the “WPT 5.7 Engineering Guide Supplement .pdf”, which is located in the WorkPlace Tech\Help folder. “.hlp” files, referred to as “Windows Help” files, are not supported in Vista, and are problematic in XP. That is why it was replaced with the functionality of Adobe documentation. As a temporary solution, create a desktop shortcut to the .pdf file for quick access.