Issue
In Niagara G3 Workbench, how can the size of the wire sheet be adjusted?
Product Line
TAC IA Series
Environment
Niagara G3 Workbench
Cause
Locating the settings to configure the Wire Sheet width and height to increase or decrease the view.
Resolution
Wire Sheet maximum size limits
Starting in NiagaraAX-3.6, you can limit the size of the wire sheet by setting size of the wire sheet in the Options dialog box.
- From the workbench main menu, select Tools > Options to open the dialog box.
- Then select the Wire Sheet option and enter a desired maximum value in the Max Width and Max Height fields, as shown, below.
- Click the OK button to complete the setting change. If you decrease the maximum wire sheet size, objects are repositioned to stay within the view, after the size change.
Note: You may need to refresh the wire sheet view to see the changes in wire sheet size and object repositioning. Also, the wire sheet borders may not be visible until you zoom out in the wire sheet view.