Issue
A large WorkPlace Tech database containing more than 250 SNVTs, for a MNL-800, compiled and saved with no issues. However, errors occur when downloading it to the controller.
Environment
- WorkPlace Tech
- MNL-800
Cause
Exceed the maximum number of 250 SNVTs, which MNL-800 support.
Resolution
The MNL-800 has a maximum capacity for 250 SNVTs. WorkPlace Tech allows more than 250 SNVTs to be added to the application and it will save and compile. However, it will not download successfully. Ensure the application contains no more than 250 SNVTs (including the default nci SNVTs) and number them 0-249.