Issue
How can I change the logo in a Xenta 7XX so it shows my company instead of TAC/Schneider Electric?
Environment
Xenta 701, 711, 721, 731
Cause
Image files are loaded with the download of a system program and default to TAC or Schneider Electric branding depending on the version. To customize them to another corporation's logo, the files must be manually edited through FTP.
Resolution
- Use ftp to get the files below from the Xenta 7xx.
- Edit the files with the new logo and rewrite them to the original location in the Xenta7xx.
- Power down/Power up the Xenta 7xx.
Logo files:
Directory www/index
- user_logotype.gif
Directory www/images
- user_logotype.gif
- s_logotype.gif
- loginlogo.gif
- 731splash.jpg (change if Xenta 731)
- 721splash.jpg (change if Xenta 721)
- 711splash.jpg (change if Xenta 711)
- 701splash.jpg (change if Xenta 701)
Note that this will be reset back to default if a new system program (firmware) is loaded.