In WorkPlace Tech 5.7.2, some selections in the menu bar at the top of the screen are missing (i.e Project and Application selections)

Issue

In WorkPlace Tech 5.7.2, some selections in the menu bar at the top of the screen are missing (i.e Project and Application selections)

Product Line

TAC I/A Series

Environment

WorkPlace Tech 5.7.2

Cause

Disable COM add-ins on the Security tab.

Resolution

  1. Click on "Tools" in the menu bar
  2. Click on "Visio Options." The Options screen appears.
  3. Click on the Security tab and un-check "Enable COM add-ins".