Issue
In Niagara G3, can the station's web login page be customized to display a custom logo?
Environment
Niagara G3
Cause
Instruction on displaying a custom logo on the station web login page.
Resolution
If the WebService of a Niagara G3 station is configured for cookie authentication (the default), the station's login page can be customized to add a custom logo, centered over the login entry field. Adding a custom logo can be done by performing the following steps:
- Go to the slot sheet of WebServices under Services in the station and add a new slot.
- Name the slot "logo", and select Type of "baja" and "Ord".
- In the property sheet of the WebServices, the new slot logo now can be used to point to an image for display on the login screen.
- The custom logo will also appear above the "Powered by NiagaraAX" when loading the Web Workbench applet.