Issue
In a Niagara G3 ENC, is there a way to view its diagnostic data without Workbench (i.e. CPU usage)? Assume the ENC is not licensed for web access.
Environment
Niagara G3 ENC
Cause
Alternative way to view the diagnostic data without Workbench.
Resolution
In a web browser, type in the following: http://x.x.x.x/ord?spy:/ (where x = IP address of the ENC) After logging in, all the diagnostic and statistical data will be available via a set of links. It's the same information that's also accessible via Workbench.