Issue
Is there a way to allow users station access, through a browser or JDE, in Niagara R2, without having to first sign-on without a user name and password?
Environment
Niagara R2
Cause
Enable "Public Access" feature to bypass sign on.
Resolution
Yes. Starting with Niagara release 2.3, a “public access” feature was added. The public access feature allows for configuration of a station to permit GxPage access without being prompted to enter a user name and password. When this feature is used, the “Sign On” dialog box is skipped and the GxPage is displayed as if user was already signed on.
See “Niagara Web Solutions Guide” for detailed setup information.