Replacement for Satchwell DWT0001 Immersion Temperature Sensor by S-E STP660 Immersion Temperature Sensor due to obsolescence.

Issue

Replacement for Satchwell DWT0001 Immersion Temperature Sensor by S-E STP660 Immersion Temperature Sensor due to obsolescence.

Product Line

Field Devices

Environment

Satchwell DWT0001 Immersion Temperature Sensor installations.

Cause

Obsolescence of Satchwell DWT0001 Immersion Temperature Sensor.

Resolution

Replace Satchwell DWT0001 Immersion Temperature Sensor with S-E STP660 Immersion Temperature Sensor.

The S-E STP660 Immersion Temperature Sensor may be used to replace the Satchwell DWT0001 Immersion Temperature Sensor, which is obsolete.

The S-E STP660 provides the same functionality as the Satchwell DWT0001, differing only in its appearance, dimensions and terminal identification.

The S-E STP660 Terminals are not polarised.

N.B.
It should be noted that the S-E STP660 is not supplied with a compatible Pocket.  The S-E STP660 stem thread however is the same as the Satchwell DWT0001 stem thread.  Should it not be possible to utilise the existing Satchwell Pocket then a S-E Pocket (9121066000-Brass or 9121060000-Stainless Steel) should be selected as appropriate to comply with the system requirements.