The communications card in a UNC 126 is the same as the NIU type 1

Issue

Is the communications card in a UNC 126 the same as the NIU type 1?

Product Line

Other

Environment

UNC 126 outstation

NIU

Cause

Need to replace the communications card of the UNC 126 with an NIU type 1.

Resolution

Yes, the communications card of the UNC 126 outstation can be replaced using the communications card from an NIU type 1.