When running Sigma 4.05 on an laptop that is also running VMware to minimize or close the application can take up to 5 seconds.

Issue

When running Sigma 4.05 on an laptop that is also running VMware to minimize or close the application can take up to 5 seconds.

Product Line

Satchwell Sigma

Environment

  • Sigma 4.05
  • VMware

Cause

Require to run the SetSigmaForVMware.exe

Resolution

The utility SetSigmaForVMware.exe has been developed to prevent the delay, but must be used on Schneider-Electric engineering laptops only. This applies to normal Windows and the VMware version where Sigma 4.05 is loaded.


Download SetSigmaForVMware utility.