Are the Network 8000, DMS, and Signal manuals available in an electronic format?

Issue

Are the Network 8000, DMS, and Signal manuals available in an electronic format?

Product Line

TAC I/A Series

Environment

  • Network 8000
  • DMS
  • Signal

Cause

Option to view Network 8000, DMS, and Signal manuals in electronic format.

Resolution

The Network 8000, DMS, and Signal manuals are available from the Publication Zone via iPortal. They are, also, available on a CD. The "Legacy zip" link downloads and extract the files, if running the program from a computer or creating the CD.

When running the program from a computer, launch "index.html" located in the extracted bin folder.

Email legacy product documentation requests to be added to the Legacy CD, to Product Support.