Plug-in 'TACOSSysPin.Document' launch failure. Unspecified error

Issue

Plug-in 'TACOSSysPin.Document' launch failure.
Unspecified error

Product Line

TAC Vista

Environment

LonMaker 3.X
TAC Vista System Plug-in

Cause

An unspecified error in the launching of the TAC Vista System Plug-in is either caused by a faulty installation or registration of the plug-in.
 

Resolution

  1. Check under Start > Settings > Control Panel > Add or Remove Programs. Look for TAC ToolPack 5.X.X.
  2. Make sure the version number 5.X.X matches the current Vista installation.
    1. If it does not, uninstall the current version of the ToolPack and install the correct version.
    2. If it is the correct version, proceed.
  3. Check the plug-in registration. In LonMaker go to LonMaker > Network Properties > Plug-in Registration. Look for TAC Vista System Plug-In (Version 5.X.X)
  4. Make sure the version number 5.X.X matches the current Vista installation.
    • If it does not, unregister the current version of the Plug-in and register the correct version.
  5. If everything appears to be installed and registered correctly, but the error persists, uninstall and reinstall the correct ToolPack. Reboot the PC, reregister the plug-in, and try to launch it again.