Issue
In Niagara G3, how can the status (up / down) of a device object be trended?
Environment
Niagara G3
Cause
Recording a connected controller's communication status
Resolution
Within the Wire Sheet that contains the device shadow object:
- Insert a StatusDemux object (from the kitControl pallet, Util folder). Link the "Status" from the device object to the "In Status" of the StatusDemux object
- Insert a Boolean Writable object. Link the "Down" slot of the StatusDemux object to the "In10" of the Boolean Writable object
- Add a BooleanCov history extension to the Boolean Writable object. This will then track the up / down status of the device.