Remote Client Configuration Issues I/Net 2.31 and prior

Issue

Remote Client Configuration Issues I.Net 2.31 and prior

Product Line

TAC I/NET

Environment

I/Net Seven version 2.xx with need for Remote Client configuration.

Equalization, FileMaster, File Master, Equalized Client, Remote Client, Equalize, FM, EQ, RC, MSDE, Express, Full SQL, SQL, TCP/IP, Connection

Cause

Remote Client changes with I/Net Seven version 2.21 to 2.31 release.

Resolution

There are two different configurations for the Remote Client setup in I/Net Seven. Clicking the links below will open a PDF document which will show how the communication should be setup.

This configuration is in the I/O Server under the current profile and can be found in the Workstation Options.

I/Net version 2.21 to 2.31

I/Net version 2.16 and prior