Issue
Update Vista Database fails. Error in the Output Build window states:
6/4/2010 12:00:00 AM Error: Operator unit object defined in TAC Network settings does not exist; Server_Name.
6/4/2010 12:00:00 AM Update Vista database failed.
Environment
TAC Vista System Plug-In
Cause
The operator unit object is the name of the Vista Server that is being updated. If the server has been renamed through Vista Server Setup or (more often) the database has been moved from PC to PC, then the default defined operator unit object may not match the current Vista database.
Resolution
Update the Operator Unit Object in the System Plug-in.
- In the System Plug-in, navigate to TAC Network > Settings... > Network > Operator unit object:
- Click the browse button (...)
- Click on the Vista Server object and hit the Select button
- Update Vista database again. The error is cleared.