Issue
In a Niagara R2 UNC-600 (or UNC-610), when using the Installation Wizard to review installed jar files, this error appears: "Cannot find distribution set platform matching the target installation platform (NT)"
Environment
- Niagara R2 UNC-600 (or UNC-610)
- Installation Wizard
Cause
The UNC-600 and UNC-610 use jar files stored in the "nt" directory. This error appears if the "emb" directory is selected instead.
Resolution
The "emb" directory is used for embedded UNCs like the UNC-410 and UNC-5x0. Selecting the "nt" directory will prevent the error from appearing and allow continuation to the jar file summary review window.