I/NET 2.31 has two different builds

Issue

Two different revisions of I/NET 2.31 were created: 2218 and 2227. How do you know which one to use?

Product Line

TAC I/NET

Environment

I/NET 2.31

Cause

Inet 2.31 was released with two different builds 2218 and 2227.

Resolution

The latest build for I/NET 2.31 is the 2227 build. If a site is running the 2218 build, it is recommended to upgrade to the later build since many functions have been greatly improved. Log in to The Exchange Download Center to download I/NET v2.31.