Issue
In Niagara G3, how can an objects value be displayed in a graphic and not its status?
Environment
Niagara G3
Cause
Default BoundLabel properties of the object are set to display the value and status. It must be adjusted to display only the value.
Resolution
In the BoundLabel properties of the object, the default text format is
%.%
This displays the value and the status of the object. To display just the object's value, edit the format to
%out.value%
The object will then display only the present value in the graphic.