Issue
In Niagara G3, how can a Boolean object's "False" condition be made to disappear?
Environment
- Niagara G3
- Boolean Object
Cause
BoundLabel properties must be adjusted for the desired operation.
Resolution
- In the BoundLabel properties of the object, right-click on the "visible" field, and choose "Animate"
- In the Animate window, click on the drop-down for the "Converter Type", and choose "I Boolean to Simple"
- Click the drop-down for the "False Value", and select "false"
- Click OK to close the Animate window
- Click OK to close the BoundLabel properties window
- Save the graphic
Now, when the object has a value of "false," it will not be visible in the graphic.